4/15/2016 5:38 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Yes ... Following are compatible with Windows 10 as per Compatibility Lists : AttachmentPCS-7_V8.2_compatibility-list_en_2016-04-14.zip (228 Downloads) |
Last edited by: Navnag at: 4/15/2016 5:56:12 AMThere is no such thing as the last bug in a program |
|
4/15/2016 5:39 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Compatibility List for WinCC V7.4 !!!
AttachmentWinCC_V7.4_compatibility-list_en_2016-04-08.zip (197 Downloads) |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
4/15/2016 7:57 AM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
RIP |
Last edited by: 1test at: 6/8/2016 9:53:00 AM~(‾▿‾)~ |
|
4/15/2016 6:22 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (927) |
Please note that the supported OS is Windows 10 Enterprise LTSB. LTSB means Long Time Service Branch and acts like older Windows versions because you still receive security updates and bugfixes through Windows update, but you not will receive enchancements and new feature updates. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on