4/19/2016 1:45 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (193) |
Your I/O-field seems to be no simple I/O-field, it's a faceplate. Do you need it to be a faceplate (for example because you don't want to change the project to much) or was this an accident? If you right-click on a normal I/O-field and select "Create faceplate" and save the faceplate it will look like that. To access the security setting of an I/O-field in a faceplate follow this FAQ:
|
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
4/19/2016 6:01 PM | |
Posts: 40 Rating: (2) |
hello arasan ! i didn't find the icons to select security screen where SHOULD I GO FIRST can you guide me to select the icons step by step thank YOU |
4/19/2016 6:05 PM | |
Posts: 40 Rating: (2) |
hello H.J it was an accident to this faceplate !! how can i do to insert password to this field ? thank YOUUUUU |
4/19/2016 6:36 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (193) |
Hello anayisse, There are to parts to securing an object: A)
B)
Once the user clicks on the I/O-field in Runtime the login-dialog pops up. If he enters his password correctly he can write a new value into the field. Please read the manual link I send you in some post above for further information. There are examples in the manual, too: |
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to1 thankful Users |
4/19/2016 10:58 PM | |
Posts: 40 Rating: (2) |
finally it works thank YOUUUUU VERY much :D |
Follow us on