4/25/2016 10:12 AM | |
Joined: 12/16/2012 Last visit: 9/13/2024 Posts: 653 Rating: (130) |
FYI
AttachmentMLFB-manual.pdf (950 Downloads) |
This contribution was helpful to2 thankful Users |
4/25/2016 10:25 AM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hello Coil Voltages are different : 3RH2140-1BE40 CONT.RELAY,4NO,DC60V CONTACTOR RELAY, 4NO, DC 60V, SIZE S00, SCREW TERMINAL CONT.RELAY,4NO,DC110V CONTACTOR RELAY, 4NO, DC 110V, SIZE S00, SCREW TERMINAL Hope this helps Cheers Navnag PS : Pl click on the links to see detailed Technical Information |
Last edited by: Navnag at: 4/25/2016 10:28:39 AMThere is no such thing as the last bug in a program |
|
This contribution was helpful to2 thankful Users |
4/25/2016 10:26 AM | |
Joined: 1/21/2016 Last visit: 9/2/2024 Posts: 43 Rating: (8) |
hii Jackcaress, Please find attach link this may lead toward your answer I am not saying that that is right answer but it can lead through right direction |
4/25/2016 10:42 AM | |
Joined: 3/12/2015 Last visit: 7/17/2024 Posts: 533 Rating: (15) |
Oke i think ive got it now, thank you for your fast responce |
This contribution was helpful to2 thankful Users |
Follow us on