4/26/2016 12:33 PM | |
Posts: 567 Rating: (107) |
Hi, this ist correct. The communication blocks will be insert by the System. |
This contribution was helpful to1 thankful Users |
4/26/2016 12:56 PM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936) |
What you want is an AS Wide interconnection. It is not just plug and play! There are some steps you must follow: The AS Wide interconnection is made automatically between two AS when you do so. In hardware configuration a step7 connection is created. You will have to download this connection. Go to NetPro and go to PLC->Load to current project->Load selected connection. Cross AS interconnections:
If one of the above preconditions cannot be fulfilled, you have to use communication blocks. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
4/26/2016 2:27 PM | |
Posts: 45 Rating: (0) |
Thank you |
Follow us on