Industry Online Support
Technical Forum
7/2/2007 1:49 PM | |
Joined: 8/10/2006 Last visit: 12/4/2023 Posts: 298 Rating: (29) |
Greetings It's been seven months since I've programmed a network of PA devices, but I don't remember having any issues. The only issue I remember is getting the device to display/transmit in PSI vs. the default of mPa, and for some reason, I couldn't change the setting through PDM. If you haven't seen it yet, perhaps this FAQ may help: Connecting a SITRANS P (DS series) to PCS7 via a PROFIBUS PA - communication -- Topic Entry ID: 766281 Edit: It just occurred to me -- is this a Siemens Sitrans, or another vendor's? If someone else's, is the data transmitted as a word where the decimal point is fixed? (for example, 23.45 mPa are transmitted as 2345) |
Last edited by: UnimogMan at: 02.07.2007 13:52 |
|
Follow us on