4/22/2016 5:12 AM |
|
Posts: 59 Rating: (9) |
I use 6ES7 231-4HD32-0XB0, Analog Input Module. At input, there is option of Voltage and Current. I wonder for Current ption with an instrument that sent 4-20mA. 1. 0 - 20 mA Setting. What is an Integer value when reading instrument which send 4mA, is it 0 or 5529.6? 2. 4 - 20 mA Setting. What is an Integer value when reading instrument which send 4mA, is it 0 or 5529.6? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/22/2016 2:11:39 PMNew subject after splitting |
|
4/22/2016 2:34 PM | |
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topic might help: Analog Values for Simatic S7-1200: TIA Portal Module 031-500 |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to3 thankful Users |
Follow us on