5/1/2016 3:32 PM | |
Posts: 2 Rating: (1) |
Hello, I have a question about how to write values to M-Bus slave from TX-Open. Normaly we read values from M-Bus meters, but in one current project we have PRO1-Mb electrical meters where we need not only read 2 tariffs but, also write command to device to change tariff. PRO1 Meter Manual says : "New data can be transferred to the meter by sending a SND_UD command. With this procedure the master transfers user data to the slave. The slave will confirm the correct receipt of data with a single character acknowledge (E5). Change tariff mode: 68 08 08 68 (53 or 73) (address) 51 09 7C 01 54 (new tariff mode same as read) (checksum) 16 " But how to make such command point in M-Bus TX-Open template? AttachmentPRO1 & PRO380 M-bus user manual.pdf (563 Downloads) |
5/2/2016 9:26 AM | |
Posts: 2 Rating: (1) |
TX-Open is a part of Siemens building automation Desigo PX system. Please see attached picture of TXOpen tool. |
Follow us on