5/6/2016 9:39 AM | |
Joined: 12/4/2009 Last visit: 4/11/2024 Posts: 452 Rating: (134) |
SMIT SALAH, no samples, but I think you should study this links: SIMATIC WinCC (TIA Portal) options (look at the bottom - SIMATIC WinCC ControlDevelopment) and: More info can probably be given by your Siemens Sales Representative. Hope this helps. |
If this post actually helped, you may consider using the Rate button above. |
|
This contribution was helpful to1 thankful Users |
5/6/2016 10:22 AM | |
Joined: 10/2/2013 Last visit: 4/15/2024 Posts: 339 Rating: (52) |
movement of a faceplate or faceplate on a PopUp screen is not possible with WinCC RT Advanced. please prefer below link for similar topic.(experts suggestions ) https://support.industry.siemens.com/tf/ww/en/posts/movable-face-plate/145446/?page=0&pageSize=10 |
Technology is best when it brings people together,so we are here now :) |
|
5/6/2016 10:40 AM | |
Joined: 7/24/2014 Last visit: 12/4/2023 Posts: 392 Rating: (66) |
Dear ankur, I was having this information but I got an information that it is possible if we can register ActiveX control of our own and if it is so we should try for it as it is something out of box And I want to just have information that how to create our own activeX control and use it and not necessary that it is useful to just move the faceplate but we would be able to add many new things if we could know how to customise it anyways thanks for answering |
Thanks and Regards |
|
Follow us on