4/29/2016 9:20 AM | |
Posts: 223 Rating: (0) |
Here are the files for the pdl (.pdl; .sav). It's the latest update On the picture, you see 'setpoint', 'percentage', 'underlimit' and 'upperlimit'. If you change the percentage, the limits change and the 'danger' and 'warning' on the gauge should also change. But the last step doesn't occur. AttachmentDrukmetingen.zip (186 Downloads) |
5/1/2016 3:09 PM | |
Posts: 223 Rating: (0) |
Ow, okay. Can you attach your altered version of the pdl? I'll take a look at it... |
5/4/2016 7:07 AM | |
Joined: 2/21/2014 Last visit: 8/13/2024 Posts: 652 Rating: (348)
|
Hi ToVerm, sorry for late reply. I was not in office initially and later I forgot :( but I attach my pdl here. I have changed the tag name without (.) for example Osprey.Act_Val to OspreyAct_Val and other's also. I removed the lines. I hardcoded the Min value = -100 and Max = 100 in the control itself. after that if I Percentage then I can see the colors changing in the Gauge control because Danger and Warning also change. //SetPropDouble(lpszPictureName,"Control3","ValueMin",0); //Return-Type: BOOL //SetPropDouble(lpszPictureName,"Control3","ValueMax",100); //Return-Type: BOOL //SetPropDouble(lpszPictureName,"Control3","Delta",0.2); //Return-Type: BOOL Thanks, HarrY AttachmentGauge.zip (191 Downloads) |
You can always use "Rate" and "To Thank" button to appreciate my efforts in helping you :) |
|
5/9/2016 11:23 AM | |
Posts: 223 Rating: (0) |
Ah, okay. Yeah, but maybe that could be the 'problem'... |
Follow us on