5/21/2009 7:07 PM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hello, Just to add and finish this thread with one FAQ. I hope will be useful. http://support.automation.siemens.com/WW/view/en/6002243 Best regards, Hristo Mihalev |
This contribution was helpful to1 thankful Users |
5/22/2009 1:45 PM | |
Joined: 8/11/2008 Last visit: 4/8/2024 Posts: 67 Rating: (22) |
to run in Vista I installed Win98SE in a VMWare machine and i can run everything, including communication (tested with tecnatron cable wit a 928B cpu and a CP1430TF) best regards. |
Roger A. Manrique |
|
This contribution was helpful to2 thankful Users |
5/22/2009 2:04 PM | |
Joined: 8/8/2008 Last visit: 12/14/2023 Posts: 78 Rating: (4) |
Thanks guys, much helped! |
This contribution was helpful to1 thankful Users |
5/9/2016 11:23 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4775 Rating: (123) |
New question published by Sky Diver840 is split to a separate thread with the subject S5 installation error, no license. Best regards |
This contribution was helpful to1 thankful Users |
Follow us on