Industry Online Support
Technical Forum
12/5/2008 7:22 AM | |
Joined: 10/3/2008 Last visit: 8/28/2024 Posts: 961 Rating: (123) |
Hello chenhaotj, yes, for a communication between PN-CPU and a third party system (wago or so) you can use the modbus block. You can download the product "OpenModbusTCP PN CPU" as a demoversion from here: S7 OpenModbusTCP. Wüstenräuber |
12/5/2008 9:36 AM | |
Joined: 9/28/2005 Last visit: 8/27/2024 Posts: 2957 Rating: (242) |
Hello, S7 OpenMODBUS/TCP PN PLC dirver license is available with order number 2XV9450-1MB02. |
Best regards, |
|
5/13/2016 12:48 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by AutoGen_1015100 is split to a separate thread with the subject Connect 3rd party to PCS7 V8.2 CPU 410-5H with Modbus TCP. Best regards |
Follow us on