3/19/2016 10:18 AM | |
Joined: 11/6/2015 Last visit: 3/4/2024 Posts: 6 Rating: (0) |
Hello everyone, I have WINCC v7.3 WITH LICENSE. and also i installed as per the procedure. But after installing when i started to run the explorer it is taking so much time to open. Around (1:30 Hour to 2:00) it is taking. so i ask you to help me out to resolve this problem. Thanks, Manjunath ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/21/2016 4:14:30 PMNew subject after splitting |
|
6/3/2016 9:07 AM | |
Posts: 2 Rating: (0) |
Hi, I had the same problem, but the solution, is you have to reintall the SQL Server 2008 R2, after that, all will be Ok, I hope you solve your problem. |
6/5/2016 7:30 AM | |
Posts: 144 Rating: (7) |
Hi Is there any Error or message during Wincc start up? may be some component needs to be installed again |
Follow us on