7/3/2015 3:01 PM | |
Joined: 2/27/2013 Last visit: 12/16/2022 Posts: 7 Rating: (0) |
Hi If I open the wincc project on the pc, there is no problem. If i open it in a Remotedesktop session, I alway have the problem, that the project doesn't open cause of the message "Project Manager can't start basis application XREF" It is WinCC V7.3 upd. 1 ---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/7/2015 10:28:46 AMNew subject after splitting |
|
6/16/2016 2:00 AM | |
Joined: 3/24/2010 Last visit: 2/29/2024 Posts: 118 Rating: (1) |
I am having the same error. I don't know what to do. I don't even connect on this PC remotely but I am having this error. "Project Manager can't start basis application XREF'' |
6/16/2016 7:09 AM | |
Joined: 10/3/2010 Last visit: 4/25/2024 Posts: 1552 Rating: (188) |
Try to create a copy of your project with another name using ProjectDuplicator and check if the copy can be opened. |
B r g d s , |
|
Follow us on