7/31/2012 3:25 PM | |
Posts: 69 Rating: (1) |
HI, I need to make the diagnostic of my CP card. I decide to use FC10 AG_CNTRL, my card is CP443-1 1EX20-0XE0, compatible with the function (https://support.automation.siemens.com/WW/adsearch/resultset.aspx?region=WW&lang=en&netmode=intranet&ui=NDAwMDAxOAAA&term=AG_CNTRL&ID=22637440&ehbid=22637440) The problem is that i want to monitor my s7connection Number 1 with an Et200S, CMD input set to 1,but there is no result 1 and 2 in output of the function. Any advice? |
7/31/2012 7:43 PM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Hi Next step depends upon the "Error" value and "Status" value ! See what these value means in attached file. Full manualhere.
Attachmentstatus.pdf (156 Downloads) |
7/31/2012 11:54 PM | |
Joined: 8/25/2005 Last visit: 3/21/2024 Posts: 1161 Rating: (110) |
Hello mrkintaro, you want to read diagnostic data of a S7 connection? Think this isn't possible with the AG_CNTRL. Checking the FAQ Which commands (CMD) of the FC10 "AG_CNTRL" are supported by the IE CPs? I read
Think there is another function to check the S7 connection Best regards Sabine |
8/1/2012 9:13 AM | |
Posts: 69 Rating: (1) |
I forgot to say also that I am using PROFINET network |
Follow us on