11/23/2012 1:28 PM | |
Posts: 1530 Rating: (59)
|
Hello Ganeshraj, could you please tell which OPC Server you are using? Is it a SIMATIC net opc.server? Please also note that WinCC OPC Server-UA kan only be used on a WinCC-Client with own project. (Compare with attachment, is was created by use of Compatibility-Tool) Nevertheless message tells us that OPC server does not support a Browser Interface. It doesn't tell something like "no connection ..., can't reach, etc. Sounds like it wouldn't be possible at all. But I must admit, that I'm not a realexpert in OPC. Best regards Bizur |
11/27/2012 1:13 PM | |
Posts: 1776 Rating: (95)
|
Hi, also have a look at WInCC information system for "WinCC OPC UA client" |
6/28/2016 7:14 PM | |
Posts: 1 Rating: (0) |
I am also trying to do the same , in my case B&R PLC is acting as server and WinCC 7.0 is acting as client . OPC UA Communication is not getting established and getting the same error . Is it required always to have the certificate for the server because in server username and password is configured , Certificate is not configured ??? Same i have tried with UA Expert - this is third party OPC Client software Connection is getting established with the PLC . Please help to resolve the issue Please find attached configuration and error images
AttachmentImages.zip (179 Downloads) |
6/29/2016 11:11 AM | |
Posts: 648 Rating: (95) |
Dear Ganeshraj, in my opinion it isn't possible to make a opc ua connection with WinCC V7.0 SP3 (look SIMATIC HMI WinCC V7.0 System description). A WinCC OPC UA-Client is possible for WinCC V7.2 and higher (Quote of System manuel WinCC V7.2: Communication: "....The OPC communication driver can be used as OPC DA client, OPC XML client, and OPC UA Client...."). Solution: Migrate your Project to WinCC V7.2 or higher or use a OPC-DA Server. With best regards rh1990 |
Last edited by: rh1990 at: 6/29/2016 11:16:56 AM |
|
6/29/2016 12:19 PM | |
Posts: 648 Rating: (95) |
Thanks for your reply. It was a new information for me. With best Regards rh1990 |
6/29/2016 1:16 PM | |
Joined: 9/19/2009 Last visit: 4/19/2024 Posts: 458 Rating: (81) |
Hi Please see the following sample, that was made with V7.0 SP3. |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
This contribution was helpful to1 thankful Users |
Follow us on