6/2/2014 11:38 AM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hello GoForIT If you have WInCC installed on a PC , Documentation for WInCC OPC Server are available in : Start->SIMATIC->WinCC->WinCC Information System ->Just search for "OPC Server" Here is a small extract below and complete manual in PDF attached. WinCC can be used as both an OPC-Server and as an OPC client. During installation of WinCC, the following WinCC OPC-Servers can be selected for installation:
For utilization of the WinCC OPC HDA, the WinCC-OPC-XML-DA server and the WinCC OPC A&E server, a license must be purchased. The "Connectivity Pack" license must be installed on the WinCC server which is utilized as the WinCC OPC HDA server, WinCC OPC XML DA server or WinCC OPC A&E server. For more information, see chapter "Licensing".
AttachmentOPC.pdf (3785 Downloads) |
There is no such thing as the last bug in a program |
|
6/2/2014 11:51 AM | |
Posts: 352 Rating: (7) |
I'm familiar with this information. When accessing the OPCServer.WinCC.1 from a client on the same computer WinCC i running. Everything is working. Connection from another cumputer in the network is not working. O |
5/19/2016 12:57 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by SaeedRadin is split to a separate thread with the subject WinCC as OPC server, can't see the server(PC1) on the bus. Best regards |
6/30/2016 8:18 AM | |
Joined: 2/27/2012 Last visit: 5/19/2024 Posts: 29 Rating: (0) |
Dear GoForIT, If you want access the Remote OPC server, DCOM configuration,Windows firewall setting need to configure in the Server and client PC. Apart from this,If you are using 64 bit operating system then have look at below post. https://msdn.microsoft.com/en-us/library/ms678426(VS.85).aspx |
Follow us on