7/2/2016 6:24 AM | |
Posts: 35 Rating: (0) |
Top. Need to help! Plz! |
7/2/2016 4:51 PM | |
Joined: 9/19/2009 Last visit: 9/25/2024 Posts: 459 Rating: (85) |
Hi All you need to do is open the ports of your router. (NAT). Do You know if you have static o dinamic public IP.? You can use www.whatismyipadress.com, and you will know your ip, after that, restart your router and try again, if you have the same ip adress, you have static IP, if you have diferent ip then you have dynamic ip. If you have dynamic IP you must configured your DNS, take a look to www.No-IP. Sample: Your local network PC:192.168.0.23 Router:192.168.0.1 Public IP: 83.245.444.543 From internet you will connect to WinCC WebNavigator across your public IP http:\83.245.444.543 By the way, you can setup https to webnavigator, this is my sample |
Last edited by: JM76 at: 7/2/2016 4:56:03 PMLast edited by: JM76 at: 7/2/2016 4:56:46 PMIf my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
This contribution was helpful to1 thankful Users |
7/4/2016 10:20 AM | |
Posts: 35 Rating: (0) |
Hi JM76, Thank for your answer. My Port of Router was NAT. I'm check port on website ping.eu, it was open. I'm still confused in this procedure. |
7/11/2016 8:19 AM | |
Posts: 648 Rating: (95) |
Good morning Step7_pro, do you know the homepage of Siemens Online Support?There you can find many FAQs and application for different themes f. e. webnavigator. I have found two FAQs and one example application for webnavigator. Perhaps it could help you to solve your problem. FAQ
Example application
If you can't find a solution contact the technical support (Linkt to Technical Support) with a sepperated service request. With best regards rh1990 |
7/18/2016 9:48 AM | |
Posts: 35 Rating: (0) |
Thank for regards. I'm success ! Nat port of modem and setup tool DNS for IP dynamic. Great! Once more, thank you. :) |
Follow us on