7/19/2016 3:25 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (193) |
Hello shibby901, I have a simple solution (which I guess you won't like too much) and a hint to a complexer solution (which isn't optimal as well). Simple solution: Change the resolution of the 24" monitors to th same resolution as the 15" Monitor and use the same resolution for the size property of your screens in the Project.
--> You need to lower the Resolution of the monitor in windows. Pro: 24" Monitor can be used without glasses from 20 meters away. Complexer solution: I guess you could use a multi client system instead of a uni client. You would always create two screens in two different resolutions. Then, when downloading to the OS, you save the 15" screens locally so your 15" client doesn't get the screen from the server but from the local path. Con: You have twice the amount of screens and if you want to change something on a screen you have to change it manually on the related one, too. I don't know enough about this, Maybe the Technical Support has a solution for you? |
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
Follow us on