7/22/2016 7:07 AM | |
Posts: 11 Rating: (0) |
Yes there are some errors. 1) The number after the letter R in the mask (R means the variable is real, like I integer, S string, etc.) it's the default value, so you mustn't have to write R//1... for the first line, R//2... for the second, etc. Only set the default value you want for the variable. In my example I set it on 1 only because value 1 was the most used. 2) Text variables are useless, you can omit them (I wrote one of them only because on the manual they use them, so I suggest you to do the same, like a single title for the mask). Another thing: I didn't see my text variable on screen when i run my program, I don't know why. The only important text is the one near every text field (in your mask "PRESS A NUMBER OPTION 1,2,3,4,5") 3) When you call R variables, at the end of the line set for everyone u1 (like rpa[u1,1], rpa[u1,2], etc.) 4) To show your mask you have to call instruction MMC only one time and set mask you want (in your example its name is SCREEN). If you do a .COM file with more masks (like //C1(SCREEN1)... //C2(SCREEN2)... etc. you can call more masks selecting the right one) I suggest you to carefully read the chapter 3.3 on the manual I linked. Also you can check this example, made by an expert (really interesting) |
This contribution was helpful to1 thankful Users |
Follow us on