3/10/2016 9:57 AM | |
Posts: 3 Rating: (0) |
Hai.. Thanks for reply. we are using this for Coal feeder application. One of the input for PLC Start is from VFD Run Feedback. We are using Relay 1 in MM 440 (Terminal 19-20) feedback to PLC. and Relay 1 is changing its state from NO to NC once stop push button released. I will try by changing P1210 to 0. attachment is for VFD connections. AttachmentSystem Diagram about coal feeder-Model.pdf (164 Downloads) |
4/24/2016 11:59 AM | |
Joined: 10/10/2010 Last visit: 4/28/2024 Posts: 307 Rating: (15) |
you can program all digital terminal for all applications |
Follow us on