8/24/2016 12:26 AM | |
Joined: 10/17/2007 Last visit: 4/22/2024 Posts: 3972 Rating: (340) |
I am still busy, find little time to read your post. Now please answer my question-- #1--What CNC system you use? #2--Do you have all 611U system data back up --in other words--if I give your the old version servo motor , you will make your m/c running in minutes? #3--Did you have master/slave issue when your old motor still good? or this issue coming to you when you use new version of servo motor?
|
If you like my comments please |
|
8/28/2016 8:55 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello _oleksandr_, I studied your machine & my observations/suggestions are as below. 1. Your axes master & slave configuration/coupling is dependent on selection of drives DI logic. So you need to study Hypertherm Micro edge pro PLC logic. This helps you to understand the machine operation logic. 2. Y & Y1 axes master slave configuration information is must. From application point of view, Y i.e. master is positioning axis & slave is speed synchronous axis. Needs to confirm from OEM. 3. Simucom U is basic tool which is for commissioning of drive. You need to set factory default parameters. Independently set Y & Y1 axis parameters & carry out optimisation. Put both the axes in operation i.e. connect to machine, modify parameters as per application i.e. as per master & slave configuration & depending upon logic drive I/O & machine should run as per the commands from CNC controller. HTH. |
Follow us on