8/30/2016 9:12 AM | |
Posts: 80 Rating: (1) |
Hello, how can I replace encoder 6SN118-1NH01-0AA0 with 6SN118-1NH01-0AA1, difference is 0AA0 and 0AA1 |
8/30/2016 10:27 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, 6SN1118-1NH01-0AA1 is control card & it is successor of 6SN1118-1NH01-0AA0. For more details click on MLFB numbers. |
8/30/2016 11:18 AM | |
Posts: 80 Rating: (1) |
Hi, I have a new 6SN1118-1NH01-0AA1, when replacement with 6SN1118-1NH01-0AA0 show me the error E0039. Should some parameters adjusted? |
8/30/2016 11:49 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Error 039 is power module identification error. Have you retained memory card module of original card while replacing with new card? Please refer the zip folder where in you will find error 039 meaning & replacement of control card procedure. HTH. Attachment611U HRS replacement .zip (147 Downloads) |
8/31/2016 2:23 AM | |
Joined: 10/17/2007 Last visit: 4/22/2024 Posts: 3972 Rating: (340) |
I think you got "new" 6SN1118-1NH01-0AA1 from some 2nd hand source--IT IS NOT BRAND NEW. YOU DID NOT mention how do you replace this control card.( they are NOT encoder but control card) the brand new card when you 1st time power up --display will showing" A1106" that means no parameters --need set up , --you need do some thing like PISCEAN showing you, or you have SIMOCOM U software, you can copy parameters from your old card (if old one not dead), then down load to the new one. --I prefer SIMOMCOM U, if your old card not dead, as this way is 100% sure and safety. (I myself have 2 time damaged my control card by replace small memory card). when you use 2nd hand card, which from other system, there are already parameters inside memory--their system using type of drive that is not march your drive, so it give you E039. you should clean all parameters if you use 2nd hand card. or you will have trouble.
|
Last edited by: nulizhang at: 8/31/2016 2:27:01 AMadd suggstion Last edited by: nulizhang at: 8/31/2016 2:27:42 AMIf you like my comments please |
|
Follow us on