4/16/2008 10:33 AM | |
Joined: 2/7/2008 Last visit: 10/3/2008 Posts: 43 Rating: (1) |
Thanks for answering, But if you look for it in the EMC Installation Guide (see attachment), pages 37/38, there are two data tables where the tittle is "max motor-drive cable length distance". I do not know if this is just related to comply to the EMC issue or what. I mean, if you select an output choke plus a filter class A drive what is the max motor-drive cable length, as you can see inTable 4-1 (page 37), these distances are justfor EMC filteredequipments (without RFI filter).Or if you seek in the catalog where the filter class A/B are shortly described. So I would like to know, if a select a drive with an RFI filter (to comply with EN 55011 or whatever) and a Iadd an output chokebecause to gete.g. 200 metersmotor-drive cable length what is wrong with my drive?Won't it comply with EMC regulationsbetween drive and supply or the installation will be a trip or what? Thanks and best greetings Attachmentmm4Appl_008_EMV_Aufbaurichtlinie_V2_1_76.pdf (252 Downloads) |
4/18/2008 9:18 AM | |
Joined: 2/7/2008 Last visit: 10/3/2008 Posts: 43 Rating: (1) |
Thanks Tractor, that's all I wanted to know. Greetings |
Follow us on