8/7/2009 8:04 AM | |
Joined: 10/7/2005 Last visit: 4/18/2024 Posts: 3003 Rating: (1046) |
hello S7Mgr insert anew "300 Station", open HWconfig and then drag you IM151-8in from the Profinet catalogue (I/O folder--> ET200S). |
Cheers |
|
This contribution was helpful to1 thankful Users |
8/7/2009 8:53 AM | |
Joined: 10/7/2005 Last visit: 4/18/2024 Posts: 3003 Rating: (1046) |
what version of PLCSIM do you use? The IM151-8 PN/DP only has Ethernet "on board", so you PLCSIM version will need to support this as the "online" PLCSIM related PG/PC interface. I have V5.4 SP3 and it works without problems, SP2 should also work (you willneed to manually setyour PG/PC interface to TCP/IP from memory), if you have SP1 orolder it may not support PLCSIM via Ethernet (I can't remember for sure, older PLCSIM version were however only capable of going "online" viaMPI). I hope this helps |
Cheers |
|
8/7/2009 8:57 AM | |
Joined: 1/22/2008 Last visit: 2/10/2022 Posts: 77 Rating: (0) |
Okie, |
7/17/2016 5:10 PM | |
Posts: 1 Rating: (0) |
After 7 years, I'am here to tell you.. thank you ! |
Last edited by: AutoGen_3928698 at: 7/17/2016 5:12:05 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on