9/14/2016 1:32 PM | |
Posts: 23 Rating: (0) |
Hi, Thank you for your answer.I have checked .the version is higher than original.that is 3. Thanks alot |
9/15/2016 10:03 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
How you transferred program? Used old MMC or new MMC? |
9/17/2016 5:33 AM | |
Posts: 23 Rating: (0) |
Hi, if you mean memory card.I used old one.I had a backup on the PG and I transfered program from PG. |
9/17/2016 4:37 PM | ||||||||||||||||||||||||||||||||||
Joined: 3/28/2015 Last visit: 8/25/2024 Posts: 721 Rating: (213) |
Hello, Kindly have a look at the following FAQ: What should you watch out for when changing from one S7-300 CPU to another?
If there are multiple differences between the order numbers, for example a CPU with the order number 6ES7315-2AF03-0AB0 is to be replaced by a CPU with the order number 6ES7315-2AG10-0AB0, then under certain circumstances you should note the following additional information: This additional information is available either in the paragraphs below or also when comparing the CPU specification and CPU properties. |
|||||||||||||||||||||||||||||||||
Eng.Mohamed Ibrahim |
||||||||||||||||||||||||||||||||||
9/21/2016 10:10 AM | |
Posts: 23 Rating: (0) |
hello, I havent seen additional information that you told.please send this information that I should note. thanks alot |
Follow us on