9/29/2016 3:57 PM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
Hi, Is it possible to use PC USB adapter (6ES7972-0CB20-0XA0) for loading an OP7 panel with Protool/Pro v6.0+SP3 ? I tried to download this but none of the leds of the adapter went on.. It's not the adapter itself , because I tried with several ones... |
9/29/2016 4:00 PM | |
Joined: 4/24/2006 Last visit: 9/19/2024 Posts: 8739 Rating: (1168)
|
Hello OmegaProjects, This is not possible. See this link: Which connector cables are available for connecting to SIMATIC Panels? You will need serial cable 6XV1440-2KH32 In the following link, you can find the pin out: Best regards, Wizard |
Last edited by: Wizard at: 9/29/2016 4:06:53 PM |
|
This contribution was helpful to1 thankful Users |
9/29/2016 4:36 PM | |
Joined: 4/24/2006 Last visit: 9/19/2024 Posts: 8739 Rating: (1168)
|
Hello OmegaProjects, Please have in mind that an USB - RS232 convertor could give some problems. See this link: Why is the connection interrupted while transferring a project with ProTool to an OP? Best regards, Wizard |
This contribution was helpful to1 thankful Users |
Follow us on