10/11/2016 6:21 PM | |
Joined: 12/18/2014 Last visit: 9/22/2024 Posts: 33816 Rating: (4201) |
Perhaps this link may help: or this |
Last edited by: ixo65 at: 10/11/2016 6:23:29 PM |
|
10/11/2016 6:32 PM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
In the hardware configuration of your PLC , you should have the S120. When you select it , you'll see in the input/output area message frames , it's possible that this has been used... another option is that they've used an input of s120 (so an output of the PLC is triggering this) either way you can cross reference the outputs and look it up in your s7-program we'll be able to help more if you would add some print screens :) How can the Safety Functions of SINAMICS S120 be activated in an existing STEP 7 Project? |
Last edited by: OmegaProjects at: 10/11/2016 6:39:36 PM |
|
Follow us on