10/13/2016 11:08 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Are you able to view MM420 in PLC hardware library? |
10/13/2016 11:19 AM | |
Joined: 11/14/2008 Last visit: 5/6/2024 Posts: 504 Rating: (22) |
MICROMASTER 4 (MM4), SINAMICS G120 (CU 2x0x): Integrating a G120 or MM4 in a STEP 7 V11 (TIA Portal)How Can You Integrate a Drive into the TIA Portal via the Device Master File (GSD)?Hi Martijnvs, Have you checked these FAQ's ? Do you see any errors, warnings... could you please send us some more information by sending some print screens ? Regards, |
Follow us on