10/3/2016 5:13 PM | |
Joined: 11/23/2015 Last visit: 4/2/2024 Posts: 14 Rating: (0) |
Hello, We have a problem in our Redundancy Safety PLC system. There are a wire break error in safety Digital output card, only occurs in active channel. The picture of the error is as below. I am using Digital output 6ES7326-2BF01-0AB0 with MTA 6ES7650-1AL11-6XX0. Type of system: Redundancy system (safety). Type of I/O card: Digital output 6ES7326-2BF01-0AB0 Type of MTA: 6ES7650-1AL11-6XX0 Type of Relay: MYN2-D (Omron) Any body can help me resolve the problem. Thanks in advance! AttachmentWire break error 326-2BF01-0AB0.docx (197 Downloads) |
10/4/2016 5:43 AM | |
Joined: 11/23/2015 Last visit: 4/2/2024 Posts: 14 Rating: (0) |
Can Any expert help me? |
10/6/2016 1:18 PM | |
Joined: 2/12/2011 Last visit: 1/30/2024 Posts: 1 Rating: (0) |
what type of load do you have on these channels,hope it is over the low limit for redundant output? |
10/6/2016 3:19 PM | |
Joined: 11/23/2015 Last visit: 4/2/2024 Posts: 14 Rating: (0) |
I use relay type MY2N-D2 of Omron, i am sure it is not over the low limit of Redundant module. |
10/25/2016 11:28 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
hi, have you already had a look to the manual of the MTA-module ET 200M Marshalled Termination Assemblies Remote I/O Modules see chapter 14 hope this helps, regards, |
FCK WAR! |
|
Follow us on