12/1/2005 5:29 PM | |
Posts: 5 Rating: (1) |
In addition to previous information, and thank you for the note to change from uss_rpm_d to uss_rpm_r fro reading 1078; Still not receiving the value to parameter 1078. Here is program status after one input from I0.0 to XMT; MM440Berr.jpg and after another input from I0.0 to XMT; MM440Aerr.jpg (both .jpg's are in .zip file) The value for the parameter 1078 indicated after first input from I0.0 is not correct. And the error #8 indicating that the port is busy after the second input from I0.0 never goes away unless I stop and start the 224XP. Appreciate you time and help. Here are the values in Starter expert list when Starter is online with 224XP using USS_RPM_R to get 1078 (MM440Cerr.jpg) and using USS_CTRL to control MM440 (MM440Derr.jpg). When trying to read values using USS_RPM_R I get only rejected telegrams and character frame errors. When using USS_CTRL, I get only error free telegrams. Starter has also reported (seldom) consistency error when connecting to MM440 but I have not been able to find out what causes this. Still appreciate all your time and help. Attachmentmm440Aerr.zip (571 Downloads) |
Last edited by: Paul at: 12/1/2005 8:14 PMLast edited by: Paul at: 12/1/2005 5:34 PM |
|
12/1/2005 8:19 PM | |
Posts: 5 Rating: (1) |
Here are the values in Starter expert list when Starter is online with 224XP using USS_RPM_R to get 1078 (MM440Cerr.jpg) and using USS_CTRL to control MM440 (MM440Derr.jpg). When trying to read values using USS_RPM_R I get only rejected telegrams and character frame errors. When using USS_CTRL, I get only error free telegrams. Starter has also reported (seldom) consistency error when connecting to MM440 but I have not been able to find out what causes this. Still appreciate all your time and help. AttachmentProjects.zip (568 Downloads) |
This contribution was helpful to1 thankful Users |
8/13/2008 12:14 AM | |
Posts: 16 Rating: (1) |
You don't get too much response from here. Why, because that commercial add-on won't work properly. I have same issues then you have. Money back, I say! |
1/6/2016 11:03 PM | |
Joined: 9/1/2005 Last visit: 3/5/2024 Posts: 4097 Rating: (193) |
New question published by pakistan plc is split to a separate thread with the subject USS Protocol and micro master440. Best regards |
My Forum is the place to personalize your profile, |
|
11/4/2016 9:17 AM | |
Joined: 8/21/2014 Last visit: 4/24/2024 Posts: 951 Rating: (13) |
New question published by Venky_7 is split to a separate thread with the subject Drive isn't receiving main setpoint via USS. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on