11/20/2010 4:21 AM | |
Posts: 2964 Rating: (478) |
Hi.... Can you switch on the I/R module alone and check? disconnect the other modules. Plug one by one module and check. I am attaching you the steps for checking the module. Normally if spindle accelrates / decelrates the energy is pump back to the mains....if I/R module is not sufficent to with stand immedaitely the it trips with the DC link Over voltage alarm. check it out.... Regards, Ekalavya Attachmentchecking procedure IR-FDD.pdf (1466 Downloads) |
This contribution was helpful to1 thankful Users |
6/27/2013 8:34 AM | |
Posts: 1 Rating: (0) |
Thank you very much for this doc. This has helped me a lot. |
11/10/2016 6:39 PM | |
Joined: 8/21/2014 Last visit: 4/23/2024 Posts: 951 Rating: (13) |
New question published by mnqe is split to a separate thread with the subject Simodrive E/R -MODUL: 5 V voltage level faulted. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on