1/2/2017 9:21 PM | |
Joined: 7/28/2015 Last visit: 3/21/2024 Posts: 72 Rating: (1) |
Hi to all I'm not able to find a way to configure multiple Logo 12/24RCE to one Logo master for create a master Start/Stop on the all Logos. On my demo project I try to configure it, but after 3 slave connection, the all network connection and used.. I have my 80G Ozone generator with the main HOST Logo 12/24RCE. With Q1 I tun ON the air compressor and the Solenoid valve and I start to compress the Ozone gas to the tube output. i1 is used as start/Stop on the Host generator and also on the all slave Logo. Now I will have multiple slave Logo 12/24RCE locate on different room and swimm pool, like 6 or more Logo. On manual seem possible to connect up to 16 device, but I can not find how to do. When one slave room logo start by pressing the i1 Input, have to turn ON the locally solenoid Valve on Q1 and also transmit the Start/stop command to the Host Logo Air compressor, to start running the compressor and open the Main solenoid valve. I ask if give a different way for this feature, just to use one channel start/stop ID for the all device to the Host. Can be used maybe one Merker and the Host will receive it? Someone can help me to find a simple solution with one demo? Thanks AttachmentAir compressor Host.zip (235 Downloads) |
1/3/2017 6:47 AM | |
Joined: 12/18/2014 Last visit: 4/19/2024 Posts: 32845 Rating: (4061)
|
Here is your corrected network project.
AttachmentAir compressor Host_V2.zip (242 Downloads) |
Follow us on