1/17/2017 11:39 PM | |
Joined: 9/3/2008 Last visit: 9/14/2024 Posts: 928 Rating: (162) |
You can make a put/get communication between a v5.5 project and a TIA project just like you would do if it was two separate 5.5 projects. First you decide in which cpu you will call the GET and PUT functions. This is where you will create an "Unspecified S7 connection". In your case it will be a Profibus type. Then you call the GET/PUT with a reference to the S7 connection. The connection can be either in the CPU in Step7 5.5 or in TIA portal. The other cpu, you do not need to create any connections in unless you also need to call GET/PUT function from this cpu also. For definining TIA portal connections, see "How you configure a connection in the TIA Portal?" |
Michael |
|
This contribution was helpful to2 thankful Users |
Follow us on