1/24/2017 11:14 AM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello, the voltage level should be <10V and the current <80mA, see attachment. You can find that information in the technical data of the CU240E-2 https://support.industry.siemens.com/cs/ww/de/view/109482994/en If you have a wire-break fault, you have to make sure, that 4mA are detected on the AI. Otherwise if a current less than 4mA is measured a wire-break is detected. |
With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on