9/19/2012 10:38 AM | |
Posts: 71 Rating: (0) |
Why isn't the files added here? |
9/19/2012 10:50 AM | |
Joined: 4/24/2006 Last visit: 4/22/2024 Posts: 8611 Rating: (1147) |
Hello bowler, Perhaps this link might help: how can you update the hardware catalog without direct internet access? or how do you update the STEP 7 hardware catalog in STEP 7 V5.2 onwards? Best regards, Wizard |
This contribution was helpful to1 thankful Users |
9/19/2012 10:54 AM | |
Joined: 11/15/2006 Last visit: 5/7/2021 Posts: 1319 Rating: (170) |
Which version of STEP7 do you use? |
Have Fun! |
|
9/19/2012 10:55 AM | |
Posts: 71 Rating: (0) |
I use Step 7 V5.4 SP1. |
9/19/2012 10:58 AM | |
Joined: 11/15/2006 Last visit: 5/7/2021 Posts: 1319 Rating: (170) |
You should upgrade to at least 5.4 Sp5. Then the HSP should be listed. |
Have Fun! |
|
9/19/2012 11:05 AM | |
Posts: 71 Rating: (0) |
Yes I saw that the those files require Step 7 V5.4 SP4 ->. How do I upgrade step7? Is it free? |
9/19/2012 11:09 AM | |
Joined: 4/24/2006 Last visit: 4/22/2024 Posts: 8611 Rating: (1147) |
Hello bowler, Here you can download: Service Pack 5 for STEP 7 V5.4 and STEP 7 Professional Edition 2006 Best regards, Wizard |
7/27/2015 3:34 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
1/27/2017 2:13 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by AutoGen_893550 is split to a separate thread with the subject Cannot install hardware updates. Best regards |
Follow us on