4/23/2015 1:53 PM | |
Posts: 5225 Rating: (1185) |
I can't explain too much - but I think the attached pictures may help. The idea is that you have a boolean bit from the PLC that triggers the HMI to send back some of its own information to a PLC tag. Does this help? AttachmentDesign Idea_Boolean trigger for extract HMI data.zip (495 Downloads) |
4/23/2015 2:21 PM | |
Posts: 18 Rating: (0) |
Hello William, It looks a bit of a workaround. But it works like a charm. :) Thank you so much ! 5 Stars for your answer. Greetings, H. |
2/2/2017 12:36 PM | |
Posts: 3 Rating: (4) |
An alternative is to set up a scheduled task with the trigger set to "User change". The event configuration should be the same as your screenshots detailed. |
Follow us on