11/28/2012 7:48 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello, Complete procdure of download from a S7 controller is previously explained here: Complete procedure of Uploading PLC S7 Project & program from PLC to PG
My notes on how to do it successfully: 1- Be sure that target CPU is supported by the version of STEP7 you are using.Update the hardware catalog is necessary. 2-If you are using PC adapter in "Select Node Address" Window, press"view" button to see all MPI networked (or Ethernet in case of using CP) CPUs and select one. Best regards Hamid Hosseini Attachmentupload.zip (1640 Downloads) |
Last edited by: hdhosseini at: 11/28/2012 8:05 PM// Upload a file |
|
This contribution was helpful to6 thankful Users |
4/15/2020 2:37 PM | |
Joined: 1/18/2014 Last visit: 7/1/2024 Posts: 1 Rating: (0) |
my friend use "'Edit Ethernet Node'' it wlil show it |
Follow us on