2/16/2017 9:14 AM | |
Joined: 3/2/2007 Last visit: 3/28/2024 Posts: 917 Rating: (5) |
are all the below surge suppressors suitable for the below contactor? can we use any of the below three for the 24vdc coil of the contactor? thank you 3RT2015-1BB41 , CONTACTOR, AC-3, 3KW/400V, 1NO, DC 24V, 3-POLE, SZ S00 SCREW TERMINAL , 18 A AC1 3RT2916-1BB00 , SURGE SUPPRESSOR, VARISTOR, AC 24...48V, DC 24...70V, F. CONT. RELAYS A. MOTOR CONT. SZ S00, 3RT2926-1JJ00 , SURGE SUPPRESSOR, VARISTOR WITH LED, AC 24...48V, DC 12...24V, FOR MOTOR CONTACTORS SZ S0, 3RT2916-1JK00 , SURGE SUPPRESSOR, VARISTOR WITH LED, AC 48...127V, DC 24...70V, F. CONT. RELAYS A. MOTOR CONT. SZ S00, |
... thank you ... |
|
2/16/2017 12:28 PM | |
Joined: 3/2/2007 Last visit: 3/28/2024 Posts: 917 Rating: (5) |
typing mistake. the following is suitable also? thank you 3RT2916-1JJ00 , SURGE SUPPRESSOR,VARISTORWITH LED, AC 24...48V, DC 12...24V, F. CONT. RELAYS A. MOTOR CONT. SZS00, |
... thank you ... |
|
Follow us on