7/29/2013 10:40 AM | |
Joined: 3/21/2006 Last visit: 3/26/2024 Posts: 10228 Rating: (1180) |
OK, the new series ASC880 are up to 250kW. Useful manuals - ACS880-01 hardware manual3AUA0000078093 ACS880 primary control program firmware manual3AUA0000085967 FPBA-01 PROFIBUS DP Adapter module3AFE68573271 Like a FB is possible to use my example from there/tf/WW/en/Posts/45481 In attachment a sample project with ACS880 and the settings of related parameters... Sorry for the Delay!
AttachmentSample.zip (1377 Downloads) |
This contribution was helpful to3 thankful Users |
7/29/2013 11:16 AM | |
Posts: 8946 Rating: (998) |
Thank you very much, Hristo!! Do you use ProfiDrive or AABdrive Profil? (Parameter 51.05)? Thanks, Jürgen. |
7/29/2013 11:27 AM | |
Joined: 3/21/2006 Last visit: 3/26/2024 Posts: 10228 Rating: (1180) |
In attachment: backup of ASC880. The file with extension prn is opening with Excel. The other file with Drive Composer.
AttachmentPara.zip (929 Downloads) |
Last edited by: UMENCHO at: 7/29/2013 12:41 PM |
|
This contribution was helpful to2 thankful Users |
7/29/2013 1:16 PM | |
Joined: 3/21/2006 Last visit: 3/26/2024 Posts: 10228 Rating: (1180) |
Recomended OS for Drive Composer is Windows 7. |
This contribution was helpful to1 thankful Users |
9/4/2013 8:09 PM | |
Posts: 8946 Rating: (998) |
Please find attached a FC for controlling ABB ACS xxx drives. Its only in german now, I hope I can do some english translation the next days. AttachmentE:\ABB_FC.ZIP (1093 Downloads) |
This contribution was helpful to2 thankful Users |
8/11/2015 1:44 PM | |
Posts: 8946 Rating: (998) |
There should be no difference between DP or PN. |
8/11/2015 3:18 PM | |
Posts: 2 Rating: (0) |
Of course... |
2/22/2017 7:29 PM | |
Posts: 64 Rating: (4) |
Hello, somebody used already ACS880 FB in TIA v13 SP1? |
This contribution was helpful to1 thankful Users |
Follow us on