11/12/2015 2:00 PM | |
Posts: 1529 Rating: (202) |
It's installed but it does not work. I uninstalled it and re-installed Startdrive_optional_sp1. Attached is the Log File. The line that concerns me is 20:34:55 |ERROR AdsWorkerForeignExe::GetInstallResult(): - -777: FILE_NOT_FOUND. Please check the corresponding log file for more detailed information No idea which log file it is referring to. I should note that my TIA is configured for both English and Chinese, if that makes a difference. AttachmentStartdrive_option_sp1 log file.txt (261 Downloads) |
11/13/2015 1:27 AM | |
Posts: 1529 Rating: (202) |
Hope this is the correct log file. I do not have the remove V47.cmd file in my /bin directory (or any .cmd files, only dll's). First time I've had an update problem. I'm re-downloading the update file in case it was somehow corrupted. AttachmentSIA_STARTDRIVE_OPTIONAL_V13@15-11-13_07-30-28 - Long.txt (232 Downloads) |
11/13/2015 4:48 AM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22228 Rating: (2980) |
Hello, i have extrac the file from my Installation. Try to copy the file to the path "C:\Program Files (x86)\Siemens\Automation\Portal V13\Bin\" an try a reinstall or uninstall and show if it works. Regards Christoph Attachmentdelete_HSP_47.zip (275 Downloads) |
This contribution was helpful to1 thankful Users |
3/8/2017 9:43 PM | |
Posts: 1 Rating: (0) |
Hi Jeff, I have the same problem and will try to install Update 2. Did you have issue with the end result? |
Follow us on