2/21/2014 3:54 PM | |
Joined: 1/22/2009 Last visit: 9/17/2024 Posts: 114 Rating: (16) |
Hi Wolka, knowyou this FAQ? What are the requirements for the operation of SIMATIC WinCC in a Windows network? http://support.automation.siemens.com/WW/view/en/868014 What me helped, disable and enable again the Networkcard. With best regards, Fess. |
3/9/2017 9:00 AM | |
Posts: 5 Rating: (1) |
Dear all, recently we had a similar issue with SIMATIC WinCC V7.4 ASIA that was configured as a multi-user project. Only one HMI Client was showing on SIMATIC Shell. Moreover, the Windows Domain authorisation did not work properly. Disable or Enable of either of the two network adapters helped to solve the issue temporarily, but this was not a sufficient solution since the issue was still present after restart of the WinCC HMI client. When finally all network adapters were removed from the PG/PC settings, the SIMATIC Shell and Windows domain authorisation started to operate properly even after restarting the WinCC HMI client. It seems that the PG/PC settings were somehow blocking the Simatic Shell. This bug might be possible to solve for the System developers at SIMATIC. Kind Regards, /Jernbro |
Last edited by: Jernbro_uh at: 3/9/2017 9:20:08 AM |
|
Follow us on