10/3/2011 4:22 AM | |
Posts: 95 Rating: (0) |
Can someone tell me how to wire this count module, how to read the counts, and give the link of this module's manual? Many thanks |
10/3/2011 8:06 AM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hello, Take a look at http://support.automation.siemens.com/WW/view/en/45977588 Best regards, Hristo Mihalev |
This contribution was helpful to1 thankful Users |
10/4/2011 1:59 AM | |
Joined: 10/7/2005 Last visit: 4/24/2024 Posts: 3004 Rating: (1046)
|
Hello AlecTek Your STL example usesGerman mnemonicsand I presume your Step 7 is set to use English mnemonics. You have two options tofix is : 1.) Replace "A" with "Q" (e.g. "PAD" becoms "PQD")and "E" with "I" (e.g. "PED" becoms "PID") OR 2.) Change you Step7 to German mnemonics (Options menu->Customize->Languages tab), type in the STL code with German mnemonicsand then change the mnemonicsback to English. I hope this helps P.S: If you are unsure about the STL command, remember that you can use <F1> to get the context sensitive help on it. |
Last edited by: fritz at: 10/4/2011 2:01 AMCheers |
|
3/17/2017 2:22 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
Best regards |
Follow us on