1/5/2017 1:23 PM | |
Posts: 14 Rating: (0) |
hello, in attachment i put the list from downloading. i don't use a Memory card. the firmware version of starter is V4.3.3.0 and the version of my drive: V4.7. but i don't think that this is the problem: because i have 2 other drive's that are the same version and there it's works without a problem. i also try to ofline select of the safety modus and try to download but it is not posssibel. AttachmentAlarms1.txt (568 Downloads) |
1/5/2017 1:29 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983)
|
Hi, wrong attachment! i don't ask for the alarmlist, i ask for all messages during the download! Regards Christoph |
1/5/2017 1:37 PM | |
Posts: 14 Rating: (0) |
hellow, i try to do an acceptance test but this don't work. this wire brake is because i select 4-20mA with detection but this signal is now off this download list, is this target system output? AttachmentOutput window1.txt (513 Downloads) |
3/18/2017 10:03 AM | |
Posts: 1 Rating: (0) |
hi, nothing works. is there a way to do a sort of hard reset? mvg, |
Follow us on