4/4/2017 12:10 PM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12869 Rating: (1641)
|
Hello OpisOm Im Sorry but the Loggin System is a totally different one in WinCC Professional you cannot compare it with the simple logging engine in WinCC Advanced. You cannot stop and Run the Taglogging in Runtime. also with ODK its not possible because the Settings you could do in the Runtime Settings, if you want to start the logging or not is a global one and you have to deactivate and activate the Runtime again. I nWinCC Professional or WinCC V7.X you have to go different ways than in Advaced. The right solution you have already found. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on