4/11/2017 1:06 PM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191)
|
If you are in the same network as your project, it is better to use the Multiuser Engineering (this is also possible with VMware). Thereby, you are working on the project directly, you can use the Master Data Library and so on. And you don't have to archive the project, copy it, retrieve the project and copy charts.
|
SIMATIC PCS 7 - Overview |
|
4/11/2017 4:16 PM | |
Joined: 9/9/2015 Last visit: 9/25/2024 Posts: 727 Rating: (278) |
One more solution, 1. archive the project in the real ES 2. retrieve it in your local station (VM) 3. modify all the changes (without compiling) , *Since you only modifying two charts, i would consider it as a minimal changes. Assuming you have tested all the function in a simulation environment, then you can retrieve back the original site archive, modify back all the changes into the archive , do not compile it. 4. Archive that project in your local station and retrieve it in the real ES, compile changes and download changes. Done. This solution could allow you to have minimal site work. Thanks. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
Follow us on