4/15/2017 5:49 PM | |
Posts: 2 Rating: (0) |
Hello I have a Micromaster 430 v2.1. when I fit the BOP display shows 5 dashes only. please see the image. What can I do for this problem? Thanks. |
4/15/2017 5:58 PM | |
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684) |
Hello Reza; Was this BOP functional and then faliled, or is this a new installation? The part number for your BOP is not apparent from your picture, so please look it up and compare it to the BOP-2 part number that the following FAQ shows as valid for a MM 430. MICROMASTER 4 (MM4) BOP/AOP: The display indicates '-----' or 'P----' If this is not the source of the problems the FAQ has 2 more suggestions that you should look at. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
4/27/2017 2:52 PM | |
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating: (477)
|
Yes, as dchartier suggested, this BOP in picture is not for MM430. It works for MM420/440. For MM430, BOP has buttons of Hand/Auto instead of reverse/Jog |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to1 thankful Users |
Follow us on