4/27/2017 1:22 PM | |
Posts: 88 Rating: (4) |
Dear Zaibkhan Please download the attached file and unzip the file.Then open the file using TIAPORTAL V13 |
This contribution was helpful to1 thankful Users |
4/28/2017 10:27 AM | |
Posts: 50 Rating: (3) |
Dear Zaibkhan For your new inputs, first configure the additional inputs to the hardware configuration with respective hardware catalog number as inserted physically. Then use that configured IO address in the scalling block of PLC programming. you can directly use the analog input address to the scaling block input parameter, provide the raw count (input) high and low limits, output (scalled) value high and low limits to that scalling block. Attach the address of the tag to the output parameter in which you want the scalled value to be placed. Afterwards you can use that scalled value in your logic. Hope this will help.. |
Follow us on