Industry Online Support
Technical Forum
5/21/2008 4:11 PM | |
Posts: 5 Rating: (0) |
Is it possible to write a single output by using the parameter type ANY? |
5/21/2008 6:44 PM | |
Posts: 2661 Rating: (279) |
Yes, this is possible. The ANY can be declared as an IN or IN_OUT. The ANY pointer contains the area pointer from bytes n+6 to n+9. |
5/27/2008 2:35 PM | |
Posts: 5 Rating: (0) |
Nice one, thanks. Also does anybody have an idea about how touse anANY on an IN inside the block? |
5/27/2008 10:52 PM | |
Posts: 2661 Rating: (279) |
The handling for IN is identical. Try attached FBexample for understanding the ANY. AttachmentANY_IN.zip (202 Downloads) |
Follow us on