5/4/2017 5:36 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi K2016, This is probably because the AnIn is a driver block. Each block can have a block attribute called S7_m_c which enables the block to sent variables to WinCC. The variables which need to be sent to WinCC must have the S7_m_c attribute as well. However,for driver blocks, the block attribute S7_m_c is not used so none of the variables can be sent to WinCC. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on