7/5/2016 6:14 PM | |
Joined: 12/18/2014 Last visit: 9/18/2024 Posts: 33790 Rating: (4197)
|
I have created a program with automatic scrolling pending alarm message texts. The program is designed for 8 alarm messages, but can be extended. AttachmentAutomatic_scroll_message_texts.zip (312 Downloads) |
This contribution was helpful to1 thankful Users |
7/6/2016 5:46 AM | |
Posts: 124 Rating: (13) |
Hello RossHall, Attached your program with a new message text. If some alarm occurs, the screen 6 shows all plants and how of then is or are in alarm state. AttachmentPlant alarm singles version 2.zip (293 Downloads) |
This contribution was helpful to1 thankful Users |
7/6/2016 10:24 AM | |
Posts: 15 Rating: (0) |
I have tweaked your new version to use green background for no faults however during an alarm it will utilise the white background and each alarm must be acknowledged to be cleared. Result. I'm very happy. I hope others will find this a useful add-on. AttachmentPlant alarm singles version 3.zip (289 Downloads) |
7/7/2016 6:28 AM | |
Posts: 124 Rating: (13) |
Hello RossHall, For I/O in the message text properties, follow these steps (see attachment): 1. Select a cell in the message grid. Select ON/OFF just above the message grid. 2. Select the input or output desidered from the menu which appears. 3. Select the I/O desidered from the menu which appears. 4. Type in the boxes whenever you want for when False and True states. Finalliy confirm with OK. See attached. Suggestions: Alarms has to be in high priority. After open blocks, use open conectors. You can change the block high to a inverter in the entry "En" of message text (one less block used). See you. AttachmentIncluding I O state in a message text 07 07 2016.zip (492 Downloads) |
This contribution was helpful to1 thankful Users |
5/9/2017 12:08 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by Shahjee is split to a separate thread with the subject Win CC Runtime to display the messages on one big TV. Best regards |
Follow us on